Native presentation engine
At startup of the project at runtime, generate an interactive session initially authenticated with the specified user
- BrowseName
- NativePresentationEngine
- SuperType
- Presentation engine(PresentationEngine)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Dynamic variables polling time | DynamicVariablesPollingTime | Duration | Time interval for the periodic reading of the dynamic link source field variables |
| Text render type | TextRenderType | Text render type | How text is rendered to the UI |
| Enable virtual keyboard | EnableVirtualKeyboard | Boolean | Enable/disable the virtual keyboard |
| Start window | StartWindow | NodeId | (Inherited from Presentation engine) |
| LoginWindow | LoginWindow | NodeId | (Inherited from Presentation engine) |
| Style sheet | StyleSheet | NodeId | (Inherited from Presentation engine) |
| Starting user | StartingUser | NodeId | (Inherited from Presentation engine) |
| Session | Session | NodeId | (Inherited from Presentation engine) |
| Sessions | UI Session | (Inherited from Presentation engine) |