View alarms in standard time zone
To view alarms in the standard time zone, you can display alarms events in the Alarm Grid and Alarm History Grid in the standard UTC time zone. Configure the time zone for the grid object in Template Libraries.
- Select
Template Libraries.
- In Template Libraries, select Widgets.
- Drag Alarm grid or Alarm history grid from Widgets to the desired node in the UI folder.
- In Template Libraries, select Close.
- In Project view, expand the alarm grid and select AlarmsDataGrid.
- in Properties, expand Timestamp.
- In the Text property, right-click Complex Dynamic Link and then select Reset value.
- Select
Change Dynamic Link. - In the Dynamic Links window, configure either:
- Alarm Grid. Expand Aliases, select , and then select the Time variable.
- Alarm History Grid. Expand Aliases, select , and then select LocalTime. After LocalTime, select
and then type Time.
- Choose Select.