Example interactive session and Presentation Engine

In this example, the start pages in the interactive sessions for User1, User2, and User3 are instances of the start page set in the Presentation Engine.

Each start page contains several instances of the same A, B and C objects. The objects are shown or hidden based on the dynamic logics of each user. Text is translated based on the user locale.