View alarms in remote local time zone
View alarms in the local time zone to view alarm events remotely.
-
Select
Template Libraries.
- In Template Libraries, drag the Alarm grid or Alarm history grid object from Widgets into a node in the UI folder.
- In Project view, select the alarm object.
- In Properties, expand Timestamp.
-
In Text, reset the current value and then select
Change Dynamic Link.
- At the bottom of the window, select Advanced...
-
In the Advanced Dynamic Link editor, select
Insert and then select Expression evaluator.
- In Expression, enter{0} + {1}
-
In the {0} DynamicLink pane, select
Change Dynamic Link and then select .
-
In {1} DynamicLink, select
Change Dynamic Link and then select .
- Choose Select.