Measurement systems
Display data in the measurement system for the locale of the current session.
Measurement systems include:
- International System of Measurement
- United States Customary System
- British Imperial System
If not otherwise specified for each user or each session, the measurement system is based on the country for the locale. The UI Session and User objects associate a measurement system with a language. For example, it-US displays text in Italian, but data in the U.S. system of measurement. You can display data in units of measure that are not standard to the measurement system or create customized measurement units.
Use the Measurement System Map editor to view units of measure for different measurement systems. To open the editor, select project root and then select
in the Map of measurement systems property.