Time zones in trend graphs
At runtime, the Trend Graphic object displays data in the X-axis in the UTC standard time zone.
Use the Reference time zone property of the graph to specify if data displays in the local time zone or the session time zone. When the Trend Graph object is connected to a Data logger, you must enable the Local time log property of the application to store data in the local time zone.