Add instances of types defined in Companion Specifications
Add instances of types defined in Companion Specifications one by one to your project.
Tip: To add all nodes from a Companion Specification, see Import nodes from NodeSet. To add selected nodes from a Companion Specification, see Add an OPC UA client.
Prerequisites
(optional) Add support for custom OPC UA Companion Specifications to FactoryTalk Optix Studio. See Import Companion Specifications.
To add a node from Companion Specifications
Right-click the object or folder to contain the node and select .
- (optional) Add optional objects to a node.
- (optional) Add collection items to a node.