OPC UA Companion Specifications
Supported Companion Specifications
- DI
- PackML
- Machinery
- Weihenstephan
- PADIM
- TMC v2
To add support for more Companion Specifications, import them into your project. If the imported Companion Specifications do not comply with the OPC UA requirements, FactoryTalk Optix Studio displays warnings.
Type view contains the available Companion Specifications nodes in the Companion specifications folder.
Limitations
| Limitation | Description |
|---|---|
|
Optional object instance declarations are not created |
For example, |
|
EU variables are duplicated when they are shared by different parents |
When vendors declare an Engineering Unit variable and reference it from multiple nodes, the Engineering Unit variables are duplicated for each node that references the Engineering Unit. |
|
Only one parent node is displayed |
If you import an information model with nodes referenced by more than one node with an Aggregates reference or Organizes reference or inherited references, you import only one node. |