Export nodes to NodeSet
Export nodes to a NodeSet XML file. Use the exported file to exchange OPC UA Companion Specifications.
Prerequisites
Add nodes to the project. See Project nodes.
To export nodes to NodeSet
-
In Project view, right-click a node to export and select Export to NodeSet.
Tip: You cannot export the root project node.
-
Select a location for the NodeSet XML file.
The selected node and child nodes are exported.
- (optional) In the export notification, select Open containing folder to navigate to the exported NodeSet XML file.
Import the NodeSet to an OPC UA server, another FactoryTalk Optix project, or browse the nodes offline in an OPC UA client.