Import nodes from NodeSet
Import all nodes from a NodeSet XML file.
Tip: Import nodes from NodeSet to import all nodes from OPC UA Companion Specifications defined in a NodeSet file. For more information, see OPC UA Companion Specifications.
Prerequisites
Obtain an XML file with NodeSet to import.
To import nodes from NodeSet
- In Project view, right-click Model folder or any of its subfolders and then select .
- Select the XML with NodeSet to import.
The imported nodes appear in the folder. If you import the nodes into the same location again, all changes to the already imported nodes are retained.