Add an OPC UA client
-
From the toolbar, select
Open dashboard page.
- Select Configure communications to devices.
- Select New OPC UA client.
- (optional) Edit the name of the OPC UA client.
- Select Next.
-
Under Properties, configure basic OPC UA client settings and select Next.
-
Server endpoint URL. The communication protocol and network address of the endpoint on the OPC UA server.
-
Minimum message security mode:
-
None. The messages may be unsigned and unencrypted.
-
Signature. The messages must be signed or signed and encrypted.
-
Signature and encryption. The messages must be signed and encrypted.
-
-
Minimum security policy:
-
None. The OPC UA client does not require any specific security policy.
-
Basic256Sha256. The OPC UA client requires this policy or a more secure policy.
-
Aes128_Sha256_RsaOaep. The OPC UA client requires this policy or a more secure policy.
-
Aes256_Sha256_RsaPss. The OPC UA client requires this policy.
-
-
Client certificate file. The public DER certificate file of the OPC UA client (X509v3).Tip: The client certificate file must be in the FTOptixApplication/ProjectFiles/PKI/Own/Certs/ folder.
-
Client private key file. The private PEM key file of the OPC UA client encoded with ASCII Base64.Tip: The client private key file must be in the FTOptixApplication/ProjectFiles/PKI/Own/Certs/ folder.
-
- Select Next.
-
Configure the NodeSet import:
- To import the NodeSet in the online mode, set the toggle to Online.
Tip: The online mode relies on the Server endpoint URL value of the OPC UA client object. Select Refresh to refresh the nodes published by the OPC UA server.
- To import tags in the offline mode, set the toggle to Offline and in File path, provide a path to the XML file with the NodeSet.
- To import the NodeSet in the online mode, set the toggle to Online.
- Select the nodes to import and then select Next.
- (optional) To configure another OPC UA client, select Configure another device and repeat the procedure.
- Select Exit.
In Project view, in the OPC-UA folder, the configured OPC UA client object appears.
-
(optional) Configure advanced OPC UA client properties. See Configure the OPC UA client.
-
(optional) Configure the nodes to import at runtime. See Import nodes at runtime.