Add optional objects to a node
Add optional objects to the objects that support them.
Tip: The available optional objects depend on the type definition of the parent object.
Prerequisites
Add nodes to the project. See Add instances of types defined in Companion Specifications.
To add optional objects to a node
Right-click an object and select .
The optional object appears under the node.