TwinCAT driver
Driver to communicate with the controller via the TwinCAT protocol
- BrowseName
- TwinCATDriver
- SuperType
- Communication driver(CommunicationDriver)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Runtime import | AllowRuntimeTagImport | Boolean | Enables the importation of the tags by the FactoryTalk Optix Application at runtime directly from the controller |