Table
Database table
- BrowseName
- Table
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Record limit | RecordLimit | UInt32 | Maximum limit of records (rows) in the table. When the limit is reached, the new data replace the old data in rotation |
| Columns | Columns | Store column | Table columns. Collection of StoreColumns. For ODBC database: Microsoft SQL Server maximum columns limit = 1000, maximum limit of characters in the column = 128; MySQL Server maximum columns limit = 1024, maximum limit of characters in the column = 64. For embedded database: maximum columns limit = 2000, maximum limit of characters in the column = 1024 |
Methods
Add column
- BrowseName
- AddColumn
Add a new column to the store
Remove column
- BrowseName
- RemoveColumn
Remove this column from the store
| Name | DataType | Description |
|---|---|---|
| Name | String | Name of the column to be removed |
Rename column
- BrowseName
- RenameColumn
Name of the column to be renamed
Insert
- BrowseName
- Insert
Isert data to the store
| Name | DataType | Description |
|---|---|---|
| ColumnNames | String | Column names for insert |
| Values | BaseDataType | List of records to be inserted |