Serial port
Represents a serial communication channel, configurable according to the protocol used by the controller, to create request/response-type or event-type protocols
- BrowseName
- SerialPort
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Port name | PortName | String | Number of the COM serial port to use for the Bridging service on which the modem is connected |
| Baudrate | Baudrate | UInt32 | Serial communication speed (Baud Rate). The communication speed value should be set to match that of the device with which you intend to communicate |
| Data size | DataSize | Byte | Number of bytes required by the communication protocol concerned |
| Parity | Parity | Parity | Parity type required by the communication protocol concerned |
| Stop bits | StopBits | Stop bits | Number of Stop bits required by the communication protocol concerned |
| Flow control | FlowControl | Flow control | Data flow control type for the communication type used. In particular, it makes it possible to adapt the communication according to the needs required at low level by the serial port of the connected device. By default, the driver sets None, that is, no flow control; however, depending on the device, it may be necessary to select a type of Flow Control (for example, in the event of an error message with code 1). The possible selections are: None: No flow control. The control is not required by the protocol. Hardware: The Flow control is managed by the serial line electrical signals (for example, RTS, CTS, and so on). XON/XOFF: the data flow control is XON/XOFF |
| Timeout | Timeout | Duration | Maximum wait time in milliseconds to receive a response from the controller |
| Low latency | LowLatency | Boolean | If enabled, minimizes the receive latency of an FTDI serial device |
| Communication status | CommunicationStatus | Communication status | Status of the serial communication |
Methods
Open
- BrowseName
- Open
Open the serial communication
Close
- BrowseName
- Close
Closes the serial communication
Read
- BrowseName
- Read
Read data from the serial communciation
| Name | DataType | Description |
|---|---|---|
| Count | UInt32 | Byte number |
| Name | DataType | Description |
|---|---|---|
| Buffer | Byte | Buffer |
Read
- BrowseName
- ReadUntil
Read data from the serial communication
| Name | DataType | Description |
|---|---|---|
| Delimiter | String | Delimiter |
| Name | DataType | Description |
|---|---|---|
| Buffer | Byte | Buffer |
Write
- BrowseName
- Write
Write data to the serial communication
| Name | DataType | Description |
|---|---|---|
| Buffer | Byte | Buffer |
Cancel read
- BrowseName
- CancelRead
Cancel the current read