RAAlarmData
- BrowseName
- RAAlarmData
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| EnableTime | DateTime | ||
| DisableTime | DateTime | ||
| SuppressTime | DateTime | ||
| UnsuppressTime | DateTime | ||
| ActiveTime | DateTime | ||
| InactiveTime | DateTime | ||
| ShelveTime | DateTime | ||
| UnshelveTime | DateTime | ||
| ActiveCount | Int32 | ||
| TagValue1 | BaseDataType | ||
| TagValue2 | BaseDataType | ||
| TagValue3 | BaseDataType | ||
| TagValue4 | BaseDataType | ||
| InputValue | BaseDataType |