| Maximum job size in bytes |
MaximumJobSizeInBytes |
UInt32 |
Maximum size of a transmission of tags from the controller (in bytes). 0 = 504 bytes (maximum value) |
| IP address |
IPAddress |
String |
Unique address of the controller on the network |
| Port |
Port |
UInt16 |
Number of the port used by the TCP-IP connection. It must match the one configured in the controller |
| Timeout |
Timeout |
Duration |
Maximum wait time in milliseconds to receive a response from the controller |
| CPU slot |
CpuSlot |
UInt32 |
Number of the slot occupied by the CPU in the controller rack |
| Operation code |
OperationCode |
Communication operation code |
(Inherited from Communication station) |
| Tags |
Tags |
Folder |
(Inherited from Communication station) |
| Types |
Types |
|
(Inherited from Communication station) |