Content synchronization mode
How to synchronize with the remote server
- BrowseName
- ContentSynchronizationModeEnum
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | No synchronization | Import and synchronization are disabled (user need to manually read and write values) |
| 1 | Import only | Imports the remote nodes at first connection without further synchronization |
| 2 | Import and synchronize values | Imports the remote nodes and keep them synched |
| 3 | Full synchronization | Imports the remote nodes and keep their structure and values synched |