Micro Controller Driver
Driver to communicate with Micro800 or MicroLogix 1400 controllers
- BrowseName
- MicroControllerDriver
- SuperType
- Communication driver(CommunicationDriver)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Controller type | ControllerType | Controller type | Either Micro800 or MicroLogix 1400 |
| Protocol | Protocol | Protocol | Ethernet or Serial communication protocol |
| Transmission mode | SerialProtocol | Transmission mode | Full duplex for simultaneous communication in both directions or Half duplex for communication one direction at a time |
| Serial port | SerialPort | String | Serial port number for the bridging service connected to the modem |
| Baud rate | Baudrate | UInt32 | RCB Serial communication speed required to match the baud rate of the target communication device |
| Data size | DataSize | Byte | Number of bytes |
| Parity | Parity | Parity | Error detection method |
| Stop bits | StopBits | Stop bits | Number of stop bits |