Event logger
Records the properties of one or more event types of interest generated by a specific node and/or by its child nodes, or by any node in the project, and stores them in a database
- BrowseName
- EventLogger
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Enabled | Enabled | Boolean | Enable/disable the recording of events |
| Locales | Locales | LocaleId | Locales of interest for storing translations of LocalizedText data in the database, typically the descriptions of the events. Each locale has an additional column in the database for each localized property. If empty, the locales are those expected by the project (Locales property of the project root node) |
| Database | Store | NodeId | Database in which to store the events data |
| Event configurations | EventConfigurations | Event configuration | Event configuration collection of objects. If empty, record events generated by any project node |
| Paths to event fields | EventFieldPaths | Path to event field | |
| Event arguments | EventArguments | ||
| Event fields to log | EventFieldsToLog | Event field to log | Properties to record of the different events of interest |