| Gateway IP |
GatewayIP |
String |
IP address of a valid CODESYS Gateway available in the network; usually, the IP address of the controller |
| Port |
Port |
UInt16 |
TCP/IP port used to connect with the controller. You can obtain the value from the CODESYS PLC Programming Environment: From the On line menu, select Communication Parameter |
| Device Name / Address |
PLCAddress |
String |
The CODESYS Controller Device Name or its IP address. The IP address can refer to the same machine that runs the driver using the local IP address or localhost |
| Timeout |
Timeout |
Duration |
Maximum wait time in milliseconds to receive a response from the controller |
| Operation code |
OperationCode |
Communication operation code |
(Inherited from Communication station) |
| Tags |
Tags |
Folder |
(Inherited from Communication station) |
| Types |
Types |
|
(Inherited from Communication station) |