Develop automatically generated UI
Develop a UI populated automatically with graphical elements based on the properties of objects in the Model folder.
Prerequisites
-
Download, extract, and copy the images into the ProjectName/ProjectFiles folder.
To develop the project
- Create a Motor object.
- Create a Kiln object.
- Create a list box.
- Create a vertical layout.
- Create the UIPopulator NetLogic.
- Implement the UIPopulator NetLogic.
- Arrange the interface elements.
- Save the project.

Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.