Develop a button that animates an SVG image
Configure an Advanced SVG Image object to animate the image at runtime.

Prerequisites
To develop the project
- Create an Advanced SVG Image.
- Create a NetLogic to animate the image.
- Create a button that animates the image.
- Arrange the interface elements.

Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.