Jump to main content
Rockwell Automation Home
FactoryTalk Optix Studio Help
  • Getting started

    Become familiar with the terminology, design concepts, and workflows present in the FactoryTalk® Optix™ environment and create your first project.

  • Creating projects

    Create a project and your application logic.

  • Extending projects

    Use C# to implement custom functionalities into your application logic.

  • Deploying projects

    Compile projects to FactoryTalk Optix Applications and then deploy the applications to target devices.

  • Tutorials

    Tutorials and short procedures to help with designing your own FactoryTalk Optix Applications.

    • Alarms tutorial

      The sample application for alarms walks you through how to configure an alarm associated with a change in temperature.

    • Aliases tutorial

      The sample application for aliases walks you through how to configure a dashboard for managing objects in the project.

    • Dynamic links tutorial

      The sample applications for UI (user interface) development walk you through how to configure measurement units based on the locale of a logged in user.

      • Develop a label with a localized engineering unit

        Create a simple interface that displays temperature in a format that is adjusted for a logged in user locale.

      • Develop a gauge with a localized engineering unit

        Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.

    • Graphic objects tutorial

      Configure graphic elements for different scenarios.

    • IoT tutorial

      Sample IoT projects.

    • Logger tutorial

      The sample applications for loggers walk you through how to configure various types of data loggers and event loggers.

    • NetLogic tutorial

      This section illustrates how to extend your projects with custom C# NetLogics.

    • OPC UA tutorial

      The sample application for OPC UA walks you through how to synchronize objects and variables between projects.

    • Reports tutorial

      The sample application for reports walks you through how to configure a PDF report that includes information from a data grid.

    • Sessions and locales tutorial

      Configure persistent user-specific settings and buttons to close the application and shut down the system.

    • Translations tutorial

      The sample applications for translations walk you through how to create a multilingual login form, and how to fetch translations from an OPC UA server.

  • 21CFR Part 11 Regulation Compliance

    Get acquainted with specific FactoryTalk® Optix setup instructions to comply with the 21 CFR Part 11 Regulation.

Dynamic links tutorial

The sample applications for UI (user interface) development walk you through how to configure measurement units based on the locale of a logged in user.

  • Develop a label with a localized engineering unit
  • Develop a gauge with a localized engineering unit

Provide Feedback

Have questions or feedback about this documentation? Please submit your feedback here.

Copyright ©2024 Rockwell Automation, Inc.
Legal Notice
Privacy & Cookies Policy