Develop a confirmation dialog
Create a confirmation dialog that displays when you select a button. This project involves the creation of a custom method invocation.
Prerequisites
To develop the project
- Create panels.
- Create a context object for the dialog.
- Create a confirmation dialog widget.
- Configure the SavePanel (type).
- Configure the ValuePanel (type).
- Arrange the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.