Create a Kiln object
Object properties will be used to generate interface elements automatically.
-
Create the Kiln object:
- In Project view, right-click Model and select .
-
Hover-over the object, select
, and enter Kiln.
-
Create five Kiln variables:
-
Configure the Motor variables types:
Tip: Graphical objects are created based on the variables types.
-
Set the Kiln variables values:
- Set the Address variable value to 192.168.0.1.
- Set the Image variable value to %PROJECTDIR%\A1_Boiler.svg.
- Set the SetPoint variable value to 100.
- Set the Temperature variable value to 27.3.