Develop a user-specific interface
Provide personalized user experience and make certain interface areas accessible only for particular user groups.
The Admin Pane is only visible for logged-in administrators.


Prerequisites
-
Configure users and groups in the following way:
User name
Password
Groups
Admin1
admin
Admins
User1
user
Users
To develop the project
- Create a change user form.
- Create a username label.
- Display an object to a user group.
- Arrange the interface elements.
- Save the project.

Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.