Create a list box
Create a list box that enables you to switch between Motor and Kiln objects.
- In Project view, right-click MainWindow (type) and select .
-
In Properties, create a dynamic link between Model and .
For more information about dynamic links, see Create dynamic links.
-
Expand Model and create a dynamic link between ItemKind and .
For more information about dynamic links, see Create dynamic links.