Create a Motor object
Object properties will be used to generate interface elements automatically.
-
Create the Motor object:
- In Project view pane, right-click theModel folder and select .
-
Hover-over the object, select
, and enter Motor.
-
Create Motor variables:
-
Configure the Motor variables types:
Tip: Graphical objects are created based on the variables types.
-
Set the Motor variables values:
- Set the Acceleration variable value to 23.9.
- Set the Address variable value to 192.168.0.1.
- Set the Address2 variable value to 10.90.0.1.
- Set the Image variable value to %PROJECTDIR%\A2_Motor-1.svg.
- Set the Speed variable value to 75.
- Set the Variable1 variable value to 35.5.