Translate a string
Translate a string so that the text for the string can be displayed in different languages.
- In Project view, expand Translations and then double-click a localization library.
- Select View translation references.
- In the row of the string to translate, select Synchronized. A new key with the same name as the string appears in the translation table.
-
(optional) Rename the key in the Translation reference page to add a key in the translation table.
Renaming a key does not remove the key with the previous name.
- Select View Translation Table.
- Add translations for the key.