Export translated strings to a CSV file
Export strings to use in the strings another project and help prevent having to recreate and translate the strings. Export translated strings to a CSV file using the predefined script in the template library.
-
In the main toolbar, select
Template Libraries.
- Select Scripts.
- Under Components, drag Translations Importer and Exporter into the project node or Translations folder.
- In Template Libraries, select Close.
- With Import and Export Translations selected, in Properties, in CSVPath, browse to select the .CSV file.
- In CharacterSeperator, select the separator.
- In Project view, right-click Import and Export Translations and then select Execute ExportTranslations.