Add a locale language to a localization dictionary
Add locale languages to a localization dictionary so you can change the language displayed for an application at runtime.
- In Project view, expand Translations and double-click a localization dictionary.
- In the localization dictionary, in the Translation table view, select Add locale.
-
Under Select the new locale, select a locale language and then select
.
- In New locales added, to add the locale to the displayed objects, select Yes.