Change the interface language
Change the interface language to display a different language throughout the FactoryTalk Optix Studio application at design time and runtime.
- To change the interface language, either:
- In Project view, select the project node and then in Properties, expand Localization and in Locales, select the language.
- Select
FactoryTalk Optix Studio Options and then in Language and Locale, select the language. - Have a different user with a different associated locale language log on.