Import translated strings from a CSV file
Imported translated strings so that you do not have to create and translate the strings in a localization dictionary for the current project. Import translated strings from a CSV file to populate the translation table.
Prerequisites
The CSV file must meet certain specifications:
- Each key and associated translations must exist in a new row.
- In each row, indicate the key and the associated translations in double quotes, separated by a comma. For example, "Key1", "Traduzione", "Translation". You can use a different separator.
- The first row must be a header. For example, "Key", "it-IT", "en-US".
To import the translated strings, use the predefined NetLogic that is available in the template library.
-
In the main toolbar, select
Template Libraries.
- In Template Libraries, select Scripts.
- In Components, drag Translations Importer and Exporter into the project node or the Translations folder.
- In Template Libraries, select Close.
- With Import and Export Translations selected, in Properties, in CSVPath, browse to select the .CSV file.
- In CharacterSeperator, select the separator.
- In Project view, right-click Import and Export Translations and then select Execute ImportTranslations.