Search for nodes
Use Search in Project view to search for and filter project nodes in the tree structure.
In Project view, perform any of the following:
- To search for project nodes, in Search, enter a search query.
- To clear the search query, in Search, select
. - To filter project nodes by type, in Search, select
and then select or clear the node types to include in the query. - To clear all filters, in Search, select
and then select Clear All Filters.
You can search for project nodes using their NodeID, by entering n: Node_ID
For example: n: 85/00000000000123456
Tip: You can also enter just the numeric string after the "/" as your search query. The string is unique for each project node.
For example: n: 00000000000123456
At least 4 characters of the NodeID are required to trigger the search. You can also search by namespace only, for example n: 8/ or n: 123/, with no length requirement, but this search may take more time.