Create an object
Create an object to add a node to the project.
-
In Project view, select the folder in which to create the object, and then select
in the Project view toolbar.
Tip: You can also right-click a folder in Project view and use the New context menu to create objects.The context menu displays objects that the folder can contain based on the folder category.
- Select the object to add to the project.
-
(optional) In Properties, select
, select Display name, and enter the display name.
-
(optional) In Properties, select
, select Description, and enter the description.
The new object appears in Project view. The hover-over tooltip shows the display name and description.