Create an object from a type
Create an object from a type. The new object instance is automatically of the same type.
- From Type view, double-click the folder with the category of objects.
- Drag the object type into a folder or object in Project view.
The new object appears in Project view.