Project Node IDs
When you save a project, the IDs of the project nodes that are not exposed through OPC UA may change to optimize performance. If the OPC UA server exposes nodes, the IDs of these nodes become fixed. They do not change when you save the project.
Note: See Terms dictionary to learn more about the nodeID definition.
Custom Node IDs
You can define custom fixed Node IDs by editing the ProjectName\Nodes\Model\Model.yaml file.
Important: Rockwell Automation recommends editing the Model.yaml file only for the most advanced users as it may lead to project corruption. Ensure to back up your project before making any changes to the Model.yamlfile. See Duplicate a project, Project backup, and Restore a project.
The following example of the Model.yaml file shows custom IDs defined for four variables:
Name: Model
Id: g=fb6543bf8c558b11ea2f5be225a426c0
Type: FolderType
Children:
- Name: Variable1
Id: g=d457b2dd5183a536fd7e00ed1de83292
Type: BaseDataVariableType
DataType: String
Value: "Variable with GUID"
- Name: Variable2
Id: "s='Custom Variable 2'"
Type: BaseDataVariableType
DataType: String
Value: "Variable with String spaced ID"
- Name: Variable3
Id: s=CustomVariable3
Type: BaseDataVariableType
DataType: String
Value: "Variable with String ID"
- Name: Variable4
Id: i=12345
Type: BaseDataVariableType
DataType: String
Value: "Variable with Integer ID"
- Name: Variable5
Id: 's="some"."name"'
Type: BaseDataVariableType
DataType: Int32
Value: 2