Restore a project
If a project is corrupted or unwanted changes are saved, you can restore an earlier version of the project.
- From the %localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\[Project Name] folder, copy the entire folder of the desired backup.
- Replace the current project folder with the backup folder.
- Open the project and verify that it is restored successfully.