Configure firewall for an OPC UA server
If an application has an OPC UA server running in Windows®, open the port specified in the Endpoint URL Server property of the OPC UA server.
Prerequisites
To configure firewall for an OPC UA server
When running a project with an OPC UA server object, if prompted, accept requests to configure a firewall rule.
runtimefirewall rule is created.