Store read operation codes
Configure the logger to store the operation codes of reading on the controller in the database.
Tip: For more information about the read operation codes, see Read operation codes.
Prerequisites
To store read operation codes
- In Project view, select a data logger object.
- In Properties, set Log operation code of each variable to True.