Read operation codes
For each reading operation of single or multiple tags, the controller generates an operation code that describes the operation result.
| Code | Description |
|---|---|
|
Good |
The reading operation is successful |
|
BadNoCommunication |
The reading operation failed because of a timeout (for example, a connection timeout). The timeout value is determined by the Timeout property of a Communication station object. |
|
BadCommunicationError |
The reading operation failed because the controller returned an error |
|
BadConfigurationError |
The reading operation failed because of a tag configuration error (for example, an invalid address) |