Display logger data
Display the data logger and event logger data in a table.
Prerequisites
Verify that the data logger or event logger is configured. See:
To display logger data
- In Project view, right-click UI and select .
- Select the Data grid object to open it in the editor.
-
From Project view, drag a Data logger or Event logger object to the Data grid object in the editor.
The Data grid object shows the data stored by the logger in the database.
-
To display the data updated in real time at runtime, configure the Update method or Auto refresh time property of the Data grid object.
Tip: Typically, the method is associated with a Button object event.