Edit a data logger
Edit an existing data logger.
Prerequisites
Either:
To edit a data logger
-
From the toolbar, select
Open dashboard page.
- In the central pane, select Configure a data logger.
- Select the data logger to edit.
- If needed, edit the logger Name and properties.
- Select Next.
-
If there is no database for the logger, create a database:
Tip: You can also right-click an existing database and select Duplicate. Duplicating a database is useful if you want to create a database based on an existing database.
- Select the database to store the logger data and select Next.
-
Select the variables that you want to log and select Next.
Tip: You can find variables by using the search field.
- Select Exit.
-
(optional) Set a deadband interval.
-
(optional) Store read operation codes.
-
(optional) Store variable reading date and time.