Add a scale line pen
Add a scale line pen to visualize the distance between two variable values.
Prerequisites
To add a scale line pen
-
Create two variables of the Number data type.
For more information, see Variables.
-
In Properties, next to Pens, select
and select Scale line pen.
-
Create dynamic links between the X and Y properties and the variables.
For more information about dynamic links, see Create dynamic links.