Add a polygon pen
Add a polygon pen to visualize the distance between values of an array variable.
Prerequisites
Add a polygon pen
-
In Project view, select or create an array variable of the Number data type.
For more information, see Variables.
For example, create a variable of the Number[2,3] data type.
- In Project view, select or create an XYChart object.
-
In Properties, next to Pens, select
and select Polygon line pen.
-
Create a dynamic link between Point array and the array variable.
For more information about dynamic links, see Create dynamic links.