Remove a dynamic link
Remove a dynamic link from a property to no longer have the property display the linked attribute. After removing the dynamic link you can reset the default value for the property.
To remove a dynamic link
- In Project view or the editor, select the graphic object that contains the property with the dynamic link.
-
In Properties, in the property that contains the dynamic link, right-click the dynamic link and select Remove link.
The dynamic link is removed from the property and the value entered for the property appears.
-
(optional) Right-click the property value and select Reset value.
The property displays its default value.