Edit a dynamic link
Edit a dynamic link to change the source variable or resolve a broken or unresolved link. Insert a placeholder such as {0} to make the link dynamic. Broken links display
in the property while unresolved links display
. Unresolved dynamic links cannot be resolved at design time, but they can be valid at runtime, for example, when setting a dynamic link that passes through a panel loader.
in the property while unresolved links display
. Unresolved dynamic links cannot be resolved at design time, but they can be valid at runtime, for example, when setting a dynamic link that passes through a panel loader.
-
To edit the dynamic link manually:
-
To edit the dynamic link by selecting a new source:
- To edit the dynamic link by dragging a new source, drag the new source onto the existing dynamic link in Properties.
- To restore a dynamic link for which you have selected the variable, right-click the property value and then select Restore link.