Parent node format

If a dynamic link is set between two nodes of the same data type, you can set the format for the parent node.

Data types of the source node used to set the parent node format include:

Source node data type Parent node format Description Example
  • Int16
  • Int32
  • Int64
  • Integer
  • UInt16
  • UInt32
  • UInt64
  • UInteger

0 (1234)

Decimal representation, without the thousands separator

7.989 ► 7989

Hexadecimal (ff)

Hexadecimal representation

45 ► 2d

Octal

Octal representation

80 ► 55

Binary

Binary representation

45 ► 10010110

FloatDouble

0,# (1234,5)

Rounding to the first decimal place

  • 59,78 ► 59,8

  • 59,2 ► 59,2

  • 3152,9 ► 3.152,9

0,## (1234,56)

Rounding to the second decimal place

  • 45,33994 ► 45,34

  • 1,8 ► 1,8

  • 1245,68 ► 1.245,68

0,### (1234,56)

Rounding to three decimal places

  • 4,5779 ► 4,578

  • 3,14 ► 3,14

  • 1528,65 ► 1.528,65

0.0 (1234.0)

Representation with exactly one decimal place

  • 5,68 ► 5,7

  • 5,1 ► 5,1

  • 9597,77 ► 9.597

0.00 (1234.00)

Representation with exactly two decimal places

  • 5,3 ► 5,30

  • 10,65 ► 10,65

  • 5789,564 ► 5.789,56

0.000 (1234.000)

Representation with exactly three decimal places

  • 70,4 ► 70,400

  • 87,7897 ► 87,790

  • 31529,7879 ► 31.529,788

DateTime

hh:mm

Date/time format, t

05:30

dd/MM/yy

Date/Time format, d

01/05/19

hh:mm:ss

Extended date time format, T

06:01:58

d MMM yyyy

Extended date, format D

1 gen 2019

dd/MM/yy, hh:mm

Extended date/time, format g

01/07/2016, 12:59

d MMM yyyy, hh:mm:ss

General date/time layout, format F

1 feb 2019, 6:15:28

yyyy-MM-ddThh:mm:ss.0000000Z

ISO 8601 Standard, format o or O

2019-01-07T00:00:00.0000000Z

Duration

[d.]hh:mm:ss[.0000000]

Format c

2.09:10:2006:10:20

[d:]h:mm:ss[,0000000]

General short format, g

4:9:10:20

d:hh:mm:ss,0000000

General extended format, G

4:09:20:15,0000000