OMRON Fins Driver
Supported controllers
The driver supports OMRON® CJ and CP controller families.
Controller tags import
You can only import tags from TXT files in the offline mode.
Before you import tags into FactoryTalk Optix Studio, from CX-Programmer, copy the symbol table into a TXT file.
For more information, refer to the product documentation.
Data types
| Controller data type | FactoryTalk Optix data type | Length | |
|---|---|---|---|
|
BOOL |
BOOL |
1 BIT |
|
|
CHANNEL |
INT16 |
2 BYTES |
|
|
COUNTER |
INT16 |
2 BYTES |
|
|
WORD |
UINT16 |
2 BYTES |
|
|
DWORD |
UINT32 |
4 BYTES |
|
|
LWORD |
UINT64 |
8 BYTES |
|
|
INT |
INT16 |
2 BYTES |
|
|
DINT |
INT32 |
2 BYTES |
|
|
UINT |
UINT16 |
2 BYTES |
|
|
UINT_BCD |
UINT16 |
2 BYTES |
|
|
UDINT |
UINT32 |
4 BYTES |
|
|
UDINT_BCD |
UINT32 |
4 BYTES |
|
|
LINT |
INT64 |
4 BYTES |
|
|
ULINT |
UINT64 |
8 BYTES |
|
|
ULINT_BCD |
UINT64 |
8 BYTES |
|
|
REAL |
FLOAT |
4 BYTES |
|
|
LREAL |
DOUBLE |
8 BYTES |
|
|
TIMER |
INT16 |
2 BYTES |
|
|
STRING |
STRING |
LENGTH |
|
|
ARRAY 1 dimensional |
Type [dimension] |
|
| Controller memory area | FactoryTalk Optix memory area | Notes |
|---|---|---|
|
CIO |
CIO area |
|
|
A |
Auxiliary area |
|
|
T |
Timer |
|
|
C |
Counter |
|
|
D |
Data Memory |
|
|
H |
Holding area |
|
|
W |
Work area |
|
|
Ex |
EM area CurrentBank |
Addresses memory location x in the current bank. |
|
Ex_y |
EM area |
Addresses memory location y in bank x. |
|
IR |
Not supported |
|
|
DR |
Not supported |
|
|
TK |
Not supported |